Part Number: TMDSLCDK6748
hello
When I create an RTSC project and try to use the GPIO_init() function in the GPIO.h file using the pdk's library, an unresolved symbol error occurs.
Please help me.
<Linking>
undefined first referenced
symbol in file
--------- ----------------
GPIO_init ./main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "test.out" not built
>> Compilation failure
makefile:140: recipe for target 'test.out' failed
gmake[1]: *** [test.out] Error 1
makefile:136: recipe for target 'all' failed
gmake: *** [all] Error 2