Hello, I can't find any section for error reporting. If it's not right place then sorry. description below.
CCS version: 5.1.0.06000
Windows 7 64-bit, with all updates
Debug session: TCI6618 simulator (but same thing happens in other cases)
Every second time I click "Debug" there is crash during program loading. First it is info "Program is not responding" and next CCS is just being closed. After restart of CCS situation repeats - first debug session works fine, but when I stop it using STOP button (red square) it can't be started again.
Generally I found both CCS 4 and 5 extremely unstable under 64-bit WIndows. There are many random crashes and CCSv4 can't start debug session even once. I'd like to mention that I'm also using latest eclipse (32-bit) with gcc, and there are no such problems.
I hope my feedback will be useful.
regards
MS