I'm trying to use CC 4.2 and Blackhawk USB560-BP for development on a DM365EVM board. When I try and connect to the target I get the error:
Error connecting to the target:
Error 0x80002240/-181
Fatal Error during: Initialization, OCS, Control,
The Blackhawk Config Utility reports that the device is working.
I don't believe there's a problem with the DM365EVM, because I'm able to run the DVSDK examples on the board.
Thanks
Robert Ernst