Hello,
I am using the DM8168 eval board. I have erased the flash and am trying to rewrite the flash. The way I read to do this is through code compose, but I cannot get code composer to connect to the A8. I get the error
Error connecting to target:
Error 0x20000220/-1260
Severe Error during: Executions, OCS,
The target device is operating in secure mode.
Debug is not allowed in this mode.
Now that the flash is erased I can't get the EVM to boot either. I tried to configure the SD card as it once was but it may not be exactly the same. Should I be able to connect to the A8 core if nothing is running and uBoot never launches?
Thanks,
Ben