Is there any way to do either of the following?
1) as a compiler command-line option, declare the default section name (".text" is the default)
2) as a linker command-file option, move all the standard library functions into a particular section
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any way to do either of the following?
1) as a compiler command-line option, declare the default section name (".text" is the default)
2) as a linker command-file option, move all the standard library functions into a particular section
Jason R Sachs said:1) as a compiler command-line option, declare the default section name (".text" is the default)
No. But in the linker command file you can do something like this ...
my_section_name_here { *(.text) } > MEMORY_RANGE
Jason R Sachs said:2) as a linker command-file option, move all the standard library functions into a particular section
Yes. See the section titled Specifying Library or Archive Members as Input to Output Sections in the C28x Assembly Tools User's Guide. Also note this error correction pertaining to that section.
Thanks and regards,
-George