Part Number: TMS320C6410
Tool/software:
I'm using CCS v3.3.
I'm using v3.3 because we don't have the manpower or the man-hours, and I haven't had any problems so far.
Computer: Windows7 32bit (using XP mode)
Antivirus software: Virus Buster
CCS version: 3.3.38.2
Emulator SEEDXDS510PLUS Emulator (used for about 5 years): Third party product
External memory Flash memory S29AL008J70TFI010 Infineon
○I don't know the details of the error.
I think it probably means that the DSP cannot be recognized from the writing environment CCS3.3...
Is there any more information or anything you can think of?
The error display is as follows.
"
Error connecting to the target:
Error 0x80000262/-1154
Fatal Error during: Memory. Execution . Initialization. OCS.
The memory at 0x00000000 continually indicated it was 'not ready'
The emulator was unable to regain control of the processor.
The processor must be reset.
Sequence ID: 0
Error Code: -1154
Error Class: 0x80000262
This is a board whose design has not changed for about 10 years.
We have been producing about 100 pieces a year,
Regarding boards produced after May 2023,
An event has occurred where the emulator for writing software cannot be connected.