Hello,
I have a project that needs to be built with XDCTools 3.20.08.88 instead of the version that comes with the default CCSv5 installation.
I first tried to get that previous version from the update manager in the help menu but it looks like the update feature is not fully functional yet, at least not for getting this old XDCTools version.
So my second approach was to select the desired XDCTools version by right clicking on the project and selecting: Refactor -> Upgrade RTSC Product Version -> More -> Select tool from file system and choosing the XDCTools 3.20.08.88 root directory. When I do so, I get the following message:

This was working before with CCSv5.1 M7.
Is there another workaround for me to force using another XDCTools version?
Thanks
Franck