Hi Champs,
Using the makefile we are buiding the libraries and then linking in the application to finally get the executables. But once i load the executables, i am not able to put breakpoint in the application as well as in the driver code.
If I can try to put breakpoint in the disassembly, it works. Even i can step through the code, bt not able to put breakpoint on a perticular line in teh source file.
I am using the same machine to build and debug the binary, even the path are same.
Tools are being used,
CCS :4.2.3.00004
DSP CG Tool: 7.3.0B3
Binary format : Coff
Any help would be appreciated.
=====================================================================================================================
The build log looks like,
E:/PROGRA~1/TEXASI~1/C6000C~1.0B3/bin/cl6x -c -qq -pdsw225 -mv6740 -mo -eo.o674 -ea.s674 --symdebug:dwarf -Dxdc_target_name__=C
674 -Dxdc_bld__profile_debug -D_DEBUG_=1 -Dxdc_cfg__header__='obj/c6748-evm/c6xdsp/debug/evm6748_i2c_sample_configuro/package/cf
g/i2csample_xem3.h' -Dxdc_target_types__=ti/targets/std.h -Dxdc_bld__vers_1_0_7_0_0 -mi10 -dCHIP_C6748 -D_LOCAL_bios_psp_i2c_
-D_LOCAL_bios_psp_psc_ -D_LOCAL_bios_psp_platform_evm6748_ -D_BUILD_bios_psp_i2c_ -D_BUILD_bios_psp_psc_ -D_BUILD_bios_psp_platfor
m_evm6748_ -IE:/PROGRA~1/TEXASI~1/C6000C~1.0B3/include -IE:/PROGRA~1/TEXASI~1/bios_6_33_00_06_eng/packages -IE:/PROGRA~1/TEX
ASI~1/xdctools_3_22_01_21/packages -IE:\PROGRA~1\TEXASI~1\PSPDRI~1/packages -IE:/PROGRA~1/TEXASI~1/edma3_lld_02_11_02_04/packages
-fr=obj/c6748-evm/c6xdsp/debug -fs=obj/c6748-evm/c6xdsp/debug -fc src/i2cSample_io.c
# Compiling src/i2cSample_main.c to obj/c6748-evm/c6xdsp/debug/i2cSample_main.o674 ...
E:/PROGRA~1/TEXASI~1/C6000C~1.0B3/bin/cl6x -ppd=obj/c6748-evm/c6xdsp/debug/.deps/i2cSample_main.P -c -qq -pdsw225 -mv6740 -mo -e
o.o674 -ea.s674 --symdebug:dwarf -Dxdc_target_name__=C674 -Dxdc_bld__profile_debug -D_DEBUG_=1 -Dxdc_cfg__header__='obj/c6748-e
vm/c6xdsp/debug/evm6748_i2c_sample_configuro/package/cfg/i2csample_xem3.h' -Dxdc_target_types__=ti/targets/std.h -Dxdc_bld__vers_
1_0_7_0_0 -mi10 -dCHIP_C6748 -D_LOCAL_bios_psp_i2c_ -D_LOCAL_bios_psp_psc_ -D_LOCAL_bios_psp_platform_evm6748_ -D_BUILD_bios_ps
p_i2c_ -D_BUILD_bios_psp_psc_ -D_BUILD_bios_psp_platform_evm6748_ -IE:/PROGRA~1/TEXASI~1/C6000C~1.0B3/include -IE:/PROGRA~1/
TEXASI~1/bios_6_33_00_06_eng/packages -IE:/PROGRA~1/TEXASI~1/xdctools_3_22_01_21/packages -IE:\PROGRA~1\TEXASI~1\PSPDRI~1/packages
-IE:/PROGRA~1/TEXASI~1/edma3_lld_02_11_02_04/packages -fr=obj/c6748-evm/c6xdsp/debug -fs=obj/c6748-evm/c6xdsp/debug -fc src/i2cSa
mple_main.c
=================================================================================================================================
Thanks and Regards,
Sandeep K