Part Number: LAUNCHXL-F2800157
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Tool/software:
Hello,
I am trying to run the FreeRtos on the Launchpad using the Syscfg Tool. When compiling, I get the following message:
[63] undefined first referenced
[64] symbol in file
[65] --------- ----------------
[66] portTICK_ISR ./syscfg/board.obj
It doesn't generate the code for the Tick_ISR.
Is there any way to automatically generate that code? Or do I have to write it manually?
Also, is there any document explaining the workflow when using the FreeRtos on SysCfg ?
Regards and thanks in advance.
Fernando