My target is a C6474, so I have MCSDK 1.0 installed for my networking (TCP/IP stack) support.
My projects currently have dependencies on the following components:
mcsdk_1_00_00_08
ndk_2_20_02_22
pdk_c64x_1_00_00_06
M5, M6, and M7 "discovered" them fine, and my project was actively using them. Tonight, I installed M8.5, and now CCS (Eclipse) won't "discover" them automatically; and even if I try to add them manually, they are not recognized. A fresh install of the MCSDK didn't help, either.
Please help ASAP! My application won't function without networking support.
Edit: To sound a little less dramatic, I can still load up M7, and all still works fine there. It's just that with M9 a couple of weeks away, and 5.1 (Final) due out by the end of next month, and I am just hoping I won't be stuck on a still slightly buggy milestone build for the remainder of my current project (which doesn't end for a couple of more years). ;-)