Other Parts Discussed in Thread: SYSBIOS
In CCSv5, what is the relationship between
- project > properties > C/C++ Build > settings > C6000 Compiler > Include Options
- project > properties > C/C++ General > Paths and Symbols
Are these two showing the same information? In 2), when you click on the "Show built-in values", where do these include directories come from? Stated another way, what is a built-in include directory and how are these set? I assume that this information is stored within the .cproject file (is this correct)?