Part Number: CODECOMPOSER
Tool/software:
Hello,
I am running CCS Theia 1.4.0.12 and C2000 SDK without additional plugins installed.
At the moment when I type in the editor uint32_t an #include <cstdint> automatically appears at the beginning of the source file.
This leads to build failure since <cstdint> does not exists in the C2000 sdk directories. Also some typedefs are getting syntax highlighting and some are not
which is extremely annoying. This bug is also present again _cpluplus symbol - C2000 microcontrollers forum - C2000︎ microcontrollers - TI E2E support forums