I have CCs installed and updated to CCS Version 4.2.3.00004,on two computers, now both have different problems.
if I go back to earliest version, which one should I select? does ti still have previous vertion available?
thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have CCs installed and updated to CCS Version 4.2.3.00004,on two computers, now both have different problems.
if I go back to earliest version, which one should I select? does ti still have previous vertion available?
thank you,
The CCSv4 versions are available for download here: http://processors.wiki.ti.com/index.php/Download_CCS#Code_Composer_Studio_Version_4_Downloads
It is always recommended to stay with the latest version since several bugs are fixed with each update. If you ran into problems after updating CCS to 4.2.3 via the Update Manager, I would suggest downloading and installing 4.2.4 into a separate, new folder and see how it works out. You can download and install the full version from the above link instead of updating through CCS.