This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5.1 Project -> Link files to Project

I just tried to link a file to my project.  It took me a long time to discover how to do it!!!  What happened to the option in the project menu?  I think it was something like Project -> Link files to Project back in CCSv4.  Can that be added back in?


For the record I was able to link in a file as follows:

  1. File -> New -> Other
  2. Select General -> File.  Click Next.
  3. Click on the project to which you want to link a file.
  4. Click "Advanced".
  5. Check the box "Link to file in the file system".
  6. Browse to the file and select it.

This is substantially harder than it used to be!  Granted, there are some nice capabilities like using variables, etc. but wow!