Other Parts Discussed in Thread: CCSTUDIO
It is my day one with ccs3.1 for a TIMS-DSP-6713 and I'm ready to put an axe through the lot. I have a very simple test program that starts with several #include statements. I have created a new project and added this simple test program, it appears in the project\Source directory. I then "scan for dependancies" and CCStudio finds all the include files and puts them in the project\Include directory. However, when I build the project the c-compiler claims is cannot find these files. This is madness and has wasted most of my day.