Hi All,
I have a very strange problem running the C6670 cycle approximate simulation model under the CCsV5 linux DebugServer batch environment. I get the following segfault:


Now the strange thing about this is that when I run this under my userid, it works fine. When it is run under anyone else's userid, the result is the segfault above. It looks like there is some initialization of the DDR memory interface and the code is trying to write into a file. The environment is the same in all cases (same PATH, same LD_LIBRARY_PATH and same CLASSPATH, same dss.sh script). The version we are currently using is: CCSV5.1M7 linux. I saw that there is a later linux version available: 5.1M8.5 that I will download. However, looking at the release notes did not reveal anything on this sort of problem. Have you seen anything like this before? Is there something special in the environment I may have missed?
Thanks,
Mark Brown