Other Parts Discussed in Thread: CONTROLSUITE
A customer is having issues with a CCS 4.2.1 install hanging:
Hi,
1. As per Pete's advice below, I SELECTED "cg tools" and UNSELECTED "dspbios".
2. I started CCS 4.2.1 installation at 7.55pm. (Pausing Antivirus) 3. System got hang at 8.26pm. (Pls refer attachment).
4. I waited till 9.45pm and did force shut down.
Here is my system config and installed softwares:
Pentium Dual-Core CPU T4500 @ 2.30 GHz, 1.96GB of RAM
uTorrent, Adobe, GoToMeeting, HP Print, Intel Graphics, Java, Kaspersky, Matlab, Microsoft .NET Framework, Microsoft Office, Microsoft Visual C++, National Instruments Software, Nero, Skype, TeamViewer, VisSim, WebWord, Winrar.
I believe my system is not unnecessarily loaded to be slow and hence I don't find anyy reason why it is getting HANGED.
TI FAEs mentioned the problem of Contro Suite installation error, not this hanging.
I shall confirm tomorrow if it is arising elsewhere. I will be in TI office tomorrow.
In my office I tried CCS 4.2.1 in 3 other desktops and it resulted the same. All is of high configurations though.
Well, the problem occurs from both set ups; the one I had downloaded from ti.com and the one in the memory stick.
I have tried both.
Thanks & Regards,
Satya.