Hi,
I've installed CCS v 5.1, which supposedly comes with out of the box support for the XDS560v2 emulator that is packaged with the EVM6678LE evaluation board. Unfortunately, my Windows system is not recognizing the driver. The Device Manager indicates a warning associated with the device and I'm unable to connect to the emulator from CCS. I've tried re-installing CCS to no avail. There is a post in FAQ of XDS560 wiki which shows how to verify that the driver is installed properly, but does not elaborate on how to fix the issue: http://processors.wiki.ti.com/index.php/XDS560v2_System_Trace#Q:_How_can_I_check_if_the_USB_driver_is_setup_correctly.3F
-Brant