Other Parts Discussed in Thread: OMAP-L138
Hello, After having worked with the 6748 EVM board and CCS 4.2 for a while I would really like to understand how to best setup/install from scratch all of the development tools so that when a new project is created, or examples are used- I do not get all kinds of linker errors. I have had this problem with every project I have created and have re-installed CCS, the BSP, NDK libraries over and and over to no avail- I am sure I am not installing things properly. I also looked at the system variables in windows XP to ensure they were set. But I have to say that the projects are always a huge hassle to deal with- and I am frustrated with manually finding every library and include file and adding them to my project (even ALL the examples do this) every time. Any expert guidance on this matter would be extremely appreciated. Mark