This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

erroe logs in CCS

Hello,

 

recently ervery time I open CCS(4.2.3.0004), there are tons of error messages(the log was attached).

I have renamed Ctools.dll to something else as a workround for the problem of CCS stuck at "removing break points;

also sometimes I got the problem saying "waiting for a task to finish",and hanging there frever, I have to end CCS using task management.

HOwever, other than the problems above, the rest functions are working.

anybody know what are happening?

 

thank you

6443.error.log

 

  • Harrison 2011 said:

    recently ervery time I open CCS(4.2.3.0004), there are tons of error messages(the log was attached).

    I have renamed Ctools.dll to something else as a workround for the problem of CCS stuck at "removing break points;


    If ctools.dll is renamed, then the error messages in the error log is expected, but they can be ignored.

    Harrison 2011 said:

    also sometimes I got the problem saying "waiting for a task to finish",and hanging there frever, I have to end CCS using task management.

     Is there a consistent sequence of steps that reproduces this? if not, it would be difficult to investigate but if can get it to happen consistently with a particular sequence of actions, please give us additional details. Also it might be worth it to try updating to 4.2.4 or even CCSv5 if that is an option for you.

  • Thanks.

    I updated CCS from 0004 to 0033, all the problems as well as error log are gone so far.

    is V5 stable now?thank you

  • Harrison 2011 said:
    is V5 stable now?

    Yes CCSv5 is stable and final release will be in early November.