This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: LP-EM-CC2340R5/CC2340R5 via Jlink failed - target is not connected/app.out: Load failed.

Other Parts Discussed in Thread: LP-EM-CC2340R5, SEGGER, LP-XDS110ET, CC2340R5

Tool/software:

Hello,

Code Composer Studio : 12.8.1.00005

When i check for update : No Updates Found

I'm trying to program the LP-EM-CC2340R5 via a Jlink.

I connected the JLINK to the board and switched to 3v3 as shown below:

I can detect the target as in the SEGGER wiki.

Basic configuration:

When I run the debug I get the following error: 

Cortex_M0P: File Loader: Verification failed: Could not write 0x00000000: target is not connected
Cortex_M0P: GEL: File: D:.........app.out: Load failed.

I'm fairly new to debug configuration, so I naively launched like this. Do I have a bug? Or is there more configuration to do?

For your information, debugging via LP-XDS110ET works correctly, but the aim is to use JLINK only.

Thanks in advance for your help!

Yohan,