Other Parts Discussed in Thread: OMAPL138
My customer has an OMAPL138 board from LogicPD and is getting the following error. I've sent them the gel files form logicpd to try as they were using there own. I've also asked them to check they have the OMAP SOM and not the 6748 SOM plugged in. However if that does not work what else should we check for?
They have CCS V4.1.2
I never use ARM before. I have no idea why it failed. The memory space is defined in the gel file:
/* Shared RAM */
GEL_MapAddStr( 0x80000000, 0, 0x00020000, "R|W|AS4", 0 ); // Shared RAM
Do you have any suggestion?