This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: CCS Theia keeps freezing on build errors

Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: LP-XDS110ET

Tool/software:

I'm using CCS Theia version 1.5.1.3 running on Windows 10 connected via USB to a LP-XDS110ET and LP-EM-CC2340R5. I'm using the BLE data stream sample project and if I modify the code such that it generates a compile error, Theia will freeze indefinitely. The only way to recover is using the Windows Task Scheduler, killing the application then restarting. Are there logs that I can look at to figure out what's hanging?