This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I'm trying to install CCSv10.3.1.00003 on a Windows 11 PC, but an error occurs midway and I can't install it.
After turning off my virus software, the same error occurs when I start the installer.
I'm using the offline installer.
In the Select Components screen, I only selected Hercules Safety MCUs.
The error is as follows.
When I check ti_emupack_9.3.0.00058_install.log, the following log is displayed.
I have the following questions:
1. How can I resolve the above error?
2. Can CCSv10.3.1.00003 be installed on a Windows 11 PC?
Matsumoto-san,
I'm trying to install CCSv10.3.1.00003 on a Windows 11 PC,
Please not that this version of CCS does not officially support Windows 11:
https://software-dl.ti.com/ccs/esd/documents/users_guide_10.3.0/ccs_overview.html#windows
CCS 11.0.0 is the first version to support Windows 11.
I suggest updating your CCS version to the latest version of CCS, which is 12.8.1.
Thank you,
ki
Ki-san
Thank you for your reply.
I knew that CCSv10.3.1 was not compatible with Windows 11 PCs.
However, I needed to install CCsv10.3.1 on a Windows 11 PC, so I asked.
I also tried to install CCSv12.8.1 on a Windows 11 PC, but a similar error occurred and I was unable to install it.
The error log is below.
Based on the error content above, the reason why CCSv10.3.1 and 12.8.1 cannot be installed on a Windows 11 PC is probably the same.
Therefore, I believe that CCSv10.3.1 can be installed on a Windows 11 PC.
Could you please tell me how to improve the error?
Thank you for trying 12.8.1. I am sorry to hear that it also failed.
I believe the error may be related to the antivirus/security software on the system. There are some known issues with McAfee and Kaspersky to name a few. What type of antivirus/security software is running and would it be possible to temporarily disable it during the installation?
If disabling is not an option, please start a private E2E conversation with me to discuss your options.
Thank you for your response.
I am currently using the following security software.
・ESET Endpoint Antivirus 11
・ESET Management Agent 10
・Fortinet Endpoint Detection and Response Platform
・Tanium Client 7.4.9.1062
I have tried turning off ESET when installing, but it did not install.
It is difficult to turn off software other than ESET.
Is there any good way to do this?