Hi,
I have 2 launch configurations in my CCS5.x project. One has a target configuration using an XDS560, the other XDS100 jtag.
I see these launch configurations in the project properties under Run/Debug settings but cannot figure out where they are stored.
I need to store launch and target configurations .ccxml files in a common location so others can reuse them.
I'm a little new to CCS5.x - Am I right in making these config files common? We are using the 8148 evm from Mistral and XDS560 and XDS100V2 jtags.
Maybe a more fundamental question: I assume since I have two separate target configurations (the jtag difference), that I also need two separate launch configurations for engineers to choose between (?)
Br,
Matt