Other Parts Discussed in Thread: LM3S1911
I'm using CCSv4.2.4.00033 to build a C project for Stellaris LM3S1911 (ARM CortexM3). I'm debugging a problem and I would like to have an absolute listing of the input C files, showing the absolute addresses. What is the easiest way to do this? I see the linker option --run_abs which I was hoping would just create these listing files, but this option alone is not producing anything for me. Does this work with he absolute lister described in the assembly language tools users guide? If so how?
By the way, I'm not 100% sure what codegen version I'm using. The CCS build options say "Code Generation tools: TI v4.6.4" and "Effective Code Generation tools: TI v4.9.0".
-Ruben