Other Parts Discussed in Thread: TMS320C6457
I didn't find any support for Lyrtech's EVM 6484 in the CCS, even though there is support for 6484 CPUs. Can I have any pointers on how to configure them on CCSv5.0.3?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320C6457
I didn't find any support for Lyrtech's EVM 6484 in the CCS, even though there is support for 6484 CPUs. Can I have any pointers on how to configure them on CCSv5.0.3?
Hello,
I had looked up that thread before posting and since I am using 5.03, the changes discussed in the thread are already included I believe as I can see the support for Lyrtech C6457 EVM as well as TMS320C6457 and TMS320TCI6484 device configs. I don't however see the support for C6484 EVM which has the TMS320TCI6484 device. the C6457 config has just the TMS320C6457 device on it.
Hello,
the C6457 and TCI6484 are more or less the same device. However, given the fact Lyrtech only sells the C6457 EVM in the mass market, we unfortunately don't have a specific configuration for the vertical TCI6484 EVM.
So the best we can recommend is to use the C6457 EVM configuration, or else build your own from scratch (recommended) following the information on this wiki page
http://processors.wiki.ti.com/index.php/Target_Configuration_-_Custom_Configurations
Unfortunately I do not have one ready to send you.
I hope this helps gets you started!
Best Regards,
Lisa