Tool/software:
Team,
Apparently both CCSv20 and CCS Theia are based on the Theia framework. CCSv12.8.x is based on Eclipse.
-What version should be used moving forward for F29H85 development?
-Will the C29 compiler, C29 device support and C29 feature metadata available available on the three CCS versions mentioned above?
The CCSv20 release notes is not available online so it is difficult to understand the difference with CCS Theia 1.5.x:
https://www.ti.com/tool/CCSTUDIO
-Regarding admin rights for SDKs installation:
Must every SDK (like MCU-SDK-F29H85x_1.00.00.00_EA2) be installed using the installer?
Or can the different components be recognized by CCS automatically (if they are copied over from another machine and assuming that the CCS version has support for the given device family)?
Thanks in advance,
Anthony