Tool/software:



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:



For the SimpleLink cc13xx_cc26xx SDK 7.41.00.17, please use the recommended CCS version,
TI Code Composer Studio: CCS-12.5.0
CCS Theia is not official supported for the SimpleLink cc13xx_cc26xx SDK, and even if you are able to import and run the examples, there is no support for ROV yet.
Siri
Hi Siri,
Thank you for your reply, downloading old version and will confirm later if that works.
Besides your answer where is this information to be obtained?
The CCS 20 supported platform mentions Sub 1Ghz, but if I understand this does not mean fully supported or just excluding the ROV?
Hope SDK support will be implemented into the much appreciated and improved VS plaform CCS platform, any confirmation this is on the roadmap?
We always recommend to use the Tools version listed in the release note for the SDK:
SimpleLink cc13xx_cc26xx SDK 7.41.00.17 Release Notes
It is on our roadmap for next year to support CCS Theia, and ROV support will also be part of this.
BR
Siri
Siri,
Thanks again for your quick and clear reply.
I will study the release notes a bit closed in the future.
I can confirm indeed the ROV works in CSS 12.5 as is to expected in hindsight.
This feels like the stone age in comparison but provides a workable solution.
Looking forward to the full intergration, keep it up!