Part Number: CODECOMPOSER
Tool/software:
Hello,
my Code Composer Studio stopped connecting to my XDS110 Debug Probe with the following error message:
(Error -260 @ 0x0) An attempt to connect to the XDS110 failed.
The point is, that everything worked fine until yesterday and suddenly stopped working. I am using a Windows 11 machine with Code Composer Stude 12.3.0.
What I know so far:
-The Debug Probe works fine on a different machine (Windows 10, also CCS 12.3.0)
-I tested 2 more XDS110 debug probes, none of them work anymore on this specific machine
-The device gets correctly listed in the windows device manager. Thus, the USB Connection is working fine. I also tried different USB-Ports with no success.
-I uninstalled & reinstalled CCS without success
-I uninstalled & reinstalled the device drivers for the debug probe without success
-I checked the xdsdfu tool with the -e command and no devices get listed (Whereas the device gets perfectly shown with the same command on my Windows 10 machine)
So far, I am running out of ideas. The nearest guess would be some kind of windows update, which bricked something internally?
Your help would be appreciated!
Kind Regards
Tim