This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi there,
In Menu > View > Editor Layout, I found two new items "Split Editor Horizontal" and "Split Editor Vertical". I test them and they behave the same as "Split Editor Down" and "Split Editor Right". I think they are duplicated and should be removed.
Robert.
I will need to investigate
Turns out that they are indeed identical and that we inherited both from the Theia IDE. The reason why the Theia IDE has both is because the Horizontal/Vertical was terminology from Eclipse IDE while the Right/Left is how it works with VS Code (which Theia IDE is based off). Looks like Theia IDE wanted people coming from both environments to feel comfortable.
I think it should be better to keep the UI consistent. Since we are using Theia platform, it should be ok to remove duplicated items.
I think it should be better to keep the UI consistent.
I agree. The duplicate behavior can be confusing.
Since we are using Theia platform, it should be ok to remove duplicated items.
We prefer to not make changes to the Theia IDE we inherit unless we have to. My impression is that eventually Theia IDE will remove the Horizontal/Vertical options and focus on VS Code compatibility.