I was able to port over CCS v4.2 legacy project in to CCS v5.1 RC2 and able to compile it just fine. But when I open the main.c file, I started getting errors. The compilation I did not show these errors. I check and all the paths are defined in the project settings.
Description Resource Path Location Type
Symbol 'Diags_USER1' could not be resolved DSP_Main.c /DSP_Board_v41 line 135 Semantic Error