This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do you like CCS4 IDE ?

Do you like CCS4 IDE ? I find it is not friendly enough to use. 

  • Ovie,

    CCSv4 is a lot different than CCSv3.3 so if you are used to 3.3 it takes some getting used to.  The reality is that for a new user it is more straight forward than 3.3.  The new CCSv5.1 release tries to simplify things to make it easier to get used to the new environment.  If you are making a switch from CCSv3.3 to a new version of CCS I would suggest that you move straight to CCSv5.

    There are some videos here that you may want to check out:

    http://processors.wiki.ti.com/index.php/Video_Tutorials_CCSv5

     

    Regards,

    John