This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Related to CCS Theia 1.5.1.
How would I run tasks defined in tasks.json or .theia-workspace in CCS Theia?
In standard Theia IDE they are under Terminal/Run Task. That seems to be missing in CCS Theia. Has this option been moved to a different menu?
Regards,
Eugene
Hi Ki,
That unfortunate. Why would you disable builtin Theia functionality? Should probably re-enabled.
Meanwhile, I have company wide build system and need to integrate its makefiles and source structure into CCS to simplify debugging set up. I can easily bring build system files into standard Theia or VS Code but not CCS.
How would you suggest I do that without tasks and workspace files in CCS?
Regards,
Eugene
Why would you disable builtin Theia functionality?
There was some debate about simplifying the user interface to hide/disable functionality that were not commonly used.
Should probably re-enabled.
Yes, we looking into doing this in a future release.
Thanks
ki
Hi Ki,
Looking forward for restoration of standard Theia functionality. Which release this is planned for?
Meanwhile there is still the question for CCS 20.01:
I have company-wide build system and need to integrate its makefiles and source structure into CCS to simplify debugging set up so developers can use source files to set BPs. So far, with .theia-workspace file and launch.json for manual project-less debug I had no success at all. How would you suggest doing that?
Regards,
Eugene
I have company-wide build system and need to integrate its makefiles and source structure into CCS to simplify debugging set up so developers can use source files to set BPs.
If I understand correctly, you have a external makefile build environment (outside CCS) and you wish to set up an environment to debug the generated executables using CCS. You would need source debug visibility where the source file correlation is set up to set source level BP, etc. Is this correct?
The target board might have multiple heterogenous TI MCUs (F28, F29, TMS570, MSPM0 etc.) meaning that ccxml file would be custom
Yes, you would need to create a custom target configuration using the target configuration editor:
The editor is similar to what was available in CCS Eclipse and similar steps apply regarding adding connections and devices:
https://dev.ti.com/tirex/explore/node?node=A__AFwYJhmnwlJWUElGChKuxg__ccs_devtools__FUz-xrs__LATEST
However, the tool in CCS 20 is more limited in that you can only add connections and devices while in CCS 20 had more customizable options of adding routers and cpus instead of devices.
Note that if that ccxml files between CCS 12.x and CCS 20.x are compatible as long as the devices are supported between the two environments.
As for:
I have company-wide build system and need to integrate its makefiles and source structure into CCS to simplify debugging set up so developers can use source files to set BPs. So far, with .theia-workspace file and launch.json for manual project-less debug I had no success at all. How would you suggest doing that?
Once you have your ccxml file created. You can launch a project-less debug session for it so that the launch for it is created in the launch.json file. You can also add the source search paths (Run -> Edit Source Paths...) to specify to the debugger where to look for source files when debugging (the debugger will search recursively). This will also be stored in the launch for the ccxml in the launch.json file (in addition to any other debug property settings).
Then the ccxml and launch.json can be shared to other users.
Hi Ki,
I hope that I have figured out how to use project-less debug with workspace files. The missing pieces are restoration of .theia-workspace tasks in CCS with proper handling of settings keys and full schema for launch.json (CODECOMPOSER: How to configure debug properties for Project-less debug? - Code Composer Studio forum - Code Composer Studio︎ - TI E2E support forums) so debugger properties can be set.
So far, I did not find use for CCS projects as they are really limited in what they can do for non-standard boards.
Thank you,
Eugene