Part Number: CODECOMPOSER
Tool/software:
I have tried various linux distributions and on all I could not install dependencies
- error is cannot execute command: supported platform required
and
- failed to check if dependencies are installed
Have not tried on osx or windows yet
Looking at the extension code I noticed hard coded 'windows' aspects (paths, apps etc)
It seems that only windows platform is coded/supported although there is no indication that would be the case
Although I have, most likely, all the external dependencies installed ( CCS various versions and the dev packs needed plus some other arm compilers) there is no obvious way to configure the extension
Pretty disappointing the path TI walks now
Regards