Part Number: CODECOMPOSER
Other Parts Discussed in Thread: UNIFLASH, LP-XDS110ET, LP-EM-CC2340R5
Tool/software:
Uniflash version: 8.8.1
Hardware: LP-XDS110ET + LP-EM-CC2340R5
I am trying to have the CC2340 running after flashed by Uniflash, I checked the "Execute selected reset after program load" and the "Run Target After Program Load/Flash Operation" boxes, but the program is still not running after being flashed. The red light on XDS110 keeps on after the program is loaded, it seems Uniflash is still holding the target.

I have tried both reset options(with and without HIB) but it does not make a difference. The "Reset Now" button does not work either. The only way to get the program running is by pressing the reset button on XDS110 board.
Why does Uniflash not reset the device after programming? Is there a way to solve this?
Best regards,
Shuyang