This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
I have tried building our software in Linux (using TI Code Gen Tools v4.1.4). But the resulting .out is different. We are actually building ROM and the rom-size and Rom start address is also different from what we get on building in Windows. I am using the same TI Code Gen Tools v4.1.4 on both Windows and Linux. The team has decided to use this version only as of now and not newer versions of TI Code Gen Tools on CCS 3.3 in Windows. Please let me know if this is expected and if there is any extra things to be considered while building on linux.
We are actually planning to switch to linux to build as it is much faster. Any help in this direction will be much appreciated.
Regards,
Aadishri
I would suggest starting by comparing the output of the 2 builds using objdiff. The utility is part of the cg_xml package, please see this wiki page for details: http://processors.wiki.ti.com/index.php/Code_Generation_Tools_XML_Processing_Scripts
A related thread on using objdiff to compare object files: http://e2e.ti.com/support/development_tools/compiler/f/343/p/142780/516080.aspx#516080