Hi,
We have downloaded the full DVD image of CCS5 and are currently using it on two PC's for evaluation. Both these machines have previously been running licenced versions of CCS4. We are currently waiting for the CCS4 licences to be updated by TI to CCS5 and in the meantime have decided to use CCS5 under the 90-day evaluation.
Once PC works fine, however the other does not give us the option to choose the 90-day evaluation licence after installation, it only provides the options for:
Activate
Free Licence (XDS100 JTAG, Onboard emulators, Linux/Android, Simulators)
Code Size Limited (for MSP430)
i.e. we do not get the evaulate option. We have tried a complete uninstall/re-install, and have also uninstalled CCS4 but to no avail. We do notice that it seems to be picking up the CCS4 licence as it says that the licence is for CCS4 and not valid for CCS5 - not sure where this file is so we can't remove it.
The only difference between the two PC's is that one is XP and the other is Win7.
Any suggestions?
Regards
Richard