This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

codegen 6.0.2 evaluation linker

Hello,

I've recently run into an issue using TI v6.0.2 Code Generation tools.  I am using a licensed version of CCS v4.2.4.  When linking, I get a "output file "projectname.out" exceeds code size limit" error.  The .map file for this build is labeled at the top with "TMS320C2000 Evaluation Linker PC v6.0.2".

If I roll back to TI v6.0.1 Code Generation tool, my project links successfully, and the .map file is labeled "TMS320C2000 Linker PC v6.0.1" (not an evaluation linker).  I'm wondering if I've there is a version of 6.0.2 available without the evaluation linker/code size limitation.

Any help would be greatly appreciated.

 

Alex