Other Parts Discussed in Thread: LM3S6965
Hello,
I have two questions/problems I am facing right now. Quick backstory- We are developing on a our custom board w/ a lm3s6965 uc and using the lm3s6965 EKM as our debugger with CCSv4.
1. My colleague is using CCS v4.2 on WinXP and I am using CCS 4.1.3 (the one that came with the EKM CD) on Win7. I've tried installing the latest production version of CCS (4.2) but I can never connect to the target when I am trying to debug, yet 4.1.3 works great for me. We are doing some calculations using doubles and noticed a word swapping issue between the versions. On my version, 4.1.3, the doubles are swapped by 32-bits in the memory view running the debugger, whereas his verison everything looks fine,
ex. His:
0x11112222 0x33334444 //right
Mine:
0x33334444 0x11112222 //wrong
What could be causing this? Is it a compiler setting and our app's are actually producing different .bin files or is it the a debugger issue and how it represents the data/variables? More importantly, why would I not be able to debug on 4.2?
2. We also noticed yesterday that my partners debugger began having issues connecting to the target. He has had no (serious) problems for several weeks now, and then all of the sudden it can no longer connect to the debugger. The only way to get around this issue is by restarting his computer, but once he terminates a debug session once, the issue arises again.
Any idea why he can no longer connect to the target now? And in general, what is the cause of the connections issue for both him and myself? I do like CCS but these tool problems keep tripping us up and are causing much grief (and little programming output), which makes program managers angry.
Thanks in advance,
Tony