Just upgraded to CCSv5 in order to stay current and thought it would be a good time just before launching into development for our in-house board design (plus get back to using the nicer editor I've been used to with more recent versions of Eclipse!).
However, I don't seem to be able to select the EVMAM1707 target any more. Immediately after importing my CCsv4 project, the IDE flagged a target configuration problem. I used to select the "Spectrum Digital DSK-EVM PLUS onboard USB Emulator", which then allowed me to tick the EVMAM1707 box & continue. In CCSv5, there are no options available if I select that emulator. Apparently the Free licence allows me to use the XDS100v2 (which I hope will arrive in the next day or so), or any Spectrum Digital EVM boards, but I'm not seeing it.
Anyone spot the obvious noob mistake? I'm sure I must be missing something simple...
Cheers, Jeremy