Hi,
A serious problem recently...
I have the following defines:
#define EINT asm(" clrc INTM")
#define DINT asm(" setc INTM")
#define NOP asm(" NOP")
#define FAUCNT_MSK 0x0F00 #define FAUCNT_SHIFT 8
#define SET_ARR_INDEX_MASK_SAFE(arr, index, mask, val) { DINT; \ NOP; \ arr[index] &= ~mask; \ arr[index] |= val; \ EINT; \ NOP;}
#define SET_FAULT_CNT(index, cnt) SET_ARR_INDEX_MASK_SAFE(faurea, index, FAUCNT_MSK, cnt)
and the following function:
u08 fauval[MAXFAUCNT];
u08 faucnt[MAXFAUCNT];
void VLVFAU_initFaultCounter(void) { s16 idx = MAXFAUCNT; // use while loop to start at the end of the array while(--idx >= 0) { // write the fault counter value back into faurea SET_FAULT_CNT(fauval[idx], (faucnt[idx]<<FAUCNT_SHIFT)); } }When I try to compile this I get the following error:[vlvfau.c] "C:\Program Files\Texas Instruments\C2000 Code Generation Tools 5.2.10\bin\cl2000" -g -pdsw225 -pden -pds9 -o3 -fr"D:/moogsoft/nvce_myENTWICKLUNG/NVCE_Q_CAN/Proj/Debug" -i"D:/moogsoft/nvce_myENTWICKLUNG/NVCE_Q_CAN/Proj/../OUT" -i"D:/moogsoft/nvce_myENTWICKLUNG/NVCE_Q_CAN/Proj/../../src/" -i"D:/moogsoft/nvce_myENTWICKLUNG/NVCE_Q_CAN/Proj/../../src/SHARED" -i"D:/moogsoft/nvce_myENTWICKLUNG/NVCE_Q_CAN/Proj/../../src/HW_DRIVER/TMS320F28x/Mo2833x_include" -i"D:/moogsoft/nvce_myENTWICKLUNG/NVCE_Q_CAN/Proj/../../src/HW_DRIVER/TMS320F28x/DSP2833x_include" -d"_DEBUG" -d"CANOPEN" -d"LITTLE_ENDIAN" -d"TMS320xx" -d"PARAM_NAME_AVAILABLE" -d"LARGE_MODEL" -ml -mn -v28 --float_support=fpu32 -mf -@"../../NVCE_Q_CAN/Proj/Debug.lkf" "vlvfau.c"INTERNAL ERROR: C:\Program Files\Texas Instruments\C2000 Code Generation Tools 5.2.10\bin\cg2000.exe experienced a segmentation fault while
processing function _VLVFAU_initFaultCounterThis is a serious problem. Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.
>> Compilation failureThe version of the tools is in attached bitmap file:All help gratefully received.Thanks,Vincent Groarke