Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TM4C123GH6PM, EK-TM4C123GXL
Tool/software:
I've just read a 2 year old locked post that asked about CCS Theia about not being able to create an empty project:https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1246889/codecomposer-theia---changing-the-device-target-or-creating-an-empty-project
There was a response from Ki asking if bringing back empty projects should be an option if the SDK doesn't include an empty project option. Yes, a blank empty project that can be configured to any device should be brought back to CCS. I've been wracking my head against the wall for the past few days thinking that I'm just missing something, but no it just doesn't exist. It's very deterring with how much effort it takes to get CCS going if you're trying to learn or relearn the software. You would think downloading the software, selecting the correct packages for the devices you're using would allow you to plug and play, but it is far from it.
I saw another suggestion that the only option to open a project is to import an existing example project from an SDK, but how does that help if you're going to overwrite everything? Eventually you'll run out of example projects to overwrite.
I'm trying to use the EK-TM4C123GXL to re-familiarize myself with CCS since the last time I used CCS was a few years ago. This board uses the TM4C123GH6PM, which gives no options for any projects.
When entering the EK-TM4C123GXL board, I get some example projects to pop up, but no luck in actually launching a new project from them.
Within "Create New Project" and selecting a given example that shows up for the board, I'm prompted with the SDK install every time, even though I've already downloaded/installed it.



I've pointed to it in the "products discovery-path", in which it doesn't show up as a discovered product.

I've learned that 2.1.4.178 isn't even the latest version, so I downloaded 2.2.0.295 and pointed to that. I'm still prompted with downloading the older version when creating a project. Why isn't the "Create New Project" page not trying to reference the new SDK? It is at least showing up in the products discovery-path.
I'm at a loss and am only making this post as a last resort in hopes to get this working.
I had some success with installing CCS 12.8.1, but within a few hours it started crashing every single time I opened the program and became unusable.