Other Parts Discussed in Thread: CCSTUDIO, MSPM0G3507
Tool/software:
Hi folks,
I've just tried installing CCS standalone on both Windows 10 as well as Linux. On both installations, when I attempt to browse the "out_of_box" demo I eventually get a window that interrupts me with "Error communicating with cloud agent".
I see: "[Violation] ide::resolveProxy took more than 30000ms" or "agentPort not ready for TICloudAgent"
So, first, how do I fix the "Error communicating with cloud agent" so I can actually get on with getting my work done?
And, second, why am I even communicating on the network or the cloud? That's unacceptable as avoiding "The Cloud" is the whole reason why I installed the standalone version. I can see if I disable my network connection that the entire CCS system appears to be completely crippled--I can't even "Create a new project". Where are the projects and support files in a downloadable form sufficient for offline usage?
Thanks.