This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5 and C2xLP Source Compatibility

Hi,

we're currently moving a (mainly assembly) project from C240x to F2803x by using the C2x compatibility mode. However, when compiling C-Code the compiler issues a lot of warnings like

WARNING! at line 163: [E0011] Expecting C2XLP direct addressing mode (@@) MOV T,*-SP[3] ; [CPU_] |60|  

WARNING! at line 21627: [W0000] Constant parsed as an octal number .dwcfi cfa_offset, 0

Compiler options are:

-v28 -mt -ml -g --c2xlp_src_compatible --cla_support=cla0 --asm_remarks --preproc_with_compile --preproc_dependency="[...]" --obj_directory="[...]" $FILE

Thus can't the compiler generate C2x intermediate assembly code from C which can then be assembled and linked to our existing assembly files and run together in C2x compatibility mode? Or am I simply missing a compiler switch? Or can I safely ignore these warnings?

Thanks!