Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I have a LaunchPad LP-MSPM0G3507 and I am starting to play with CCS (Version: 20.1.0.6__1.7.0)
But I am not able to modify the stack size.
I see that in generated file device_linker.cmd, stack size is 512 (--stack_size=512)
I have tried to set value 1024 for "Set C system stack size" in Properties/Build/Tools/Arm Linker/Basic Options (initially, the field "Set C system stack size" was empty)

But after a rebuild, stack size remains to 512 in device_linker.cmd or .map file.
Did I miss something ?
Regards
Jerome