Part Number: CODECOMPOSER
Tool/software:
Hi,
I´m recently switch to CCS 20.01.0.6 (Theia) and have been using CCS 12.8.1 before. My project has a directory with general information and then subdir with the same name where the CCS project resides. Like Workspace/Myproject/Myproject.
This structure has been working for years in CCS 12 and below. Then I`ve moved to CCS 20 Theia. So I set up my workspace. Copyed the project over and imported the project via the import function. Every thing was working perfect after that but after a restart of CCS the project was still there but not recognized as a CCS project. So no build or debug possible. After a re-import the project could be build again but that is only persistent until you shutdown CCS.
This is not a big problem but maybe something that could be easily fixed?!
Thanks!
Best regards
Steffen