Hello TI,
I've just installed CCS v5.1. I do not have a license for it yet. I thought there is a 90 day trial period where I can use JTAG emulators such as a Spectrum Digital XDS510 USB. When trying to debug a project I get a "License cannot be acquired" notice and the debugging session terminates.
During installation I was asked to choose from a list of three options. 1) Use the 90 day trial version 2) Unlimited use but with only the XDS100 emulator 3) Can't remember the third option. I didn't choose an option but decided to quit CCS for the day. Will I need to re-install CCS and choose option 1 in order to use the XDS510 for 90 days?
Thank you
Glen Crowder