hi,
We are using TMS570 Processor and CCS V4 as IDE for the avionics project.
As per the project requirement, we need to program the Flash memory with config data file (2K bytes) that allows
the main program to be configured for the functionality required by a specific unit with up to 32 aircraft settings
available.
Is there any tool in the CCV4 which allows to program flash memory and creates a out/hex file which can be loaded to target using nowflash ?
Or
Please suggest me if i can do task using CCV4.
suggestions are wecome.