This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 4.2.4.00033 and 5505 eZusb ***program has terminated***



Hello gents,

I am brand new here, so I think my question is going to be a simple one. When I debug my application on eZusb platform ( it is simple example that TI provides to learn it out, the music comes to IN and goes directly to OUT) after 10 minutes of running it on USB stick 5505 I got a message like:

 

 

Running Getting Started Project

<-> Audio Loopback from Stereo IN --> to HP/Lineout

Sampling frequency 48000 Hz Gain = 30 dB

 

 

and after 10 minutes:

 

**PROGRAM HAS TERMINATED**

 

Looks like CCS 4 by itself terminates my application after 10 minutes. Is that correct? How am I suppose to use the stick if after such a time the stick is terminated?

Was thinking that if I RUN the target application it must run and run.

P.S> posted it to 5505 eZusb group forum but think was wrong,

 

Regards

Many thanks.